AXIS#.SAFEPARAM.SSR_#.TIMEDELAYDECMONITORING

Description

Indicates the delay before starting the deceleration monitoring. The delay starts elapsing when Safe Speed Range (SSR) is activated. When it finally elapses, the monitoring is started. This parameter can only be used when the deceleration monitoring is enabled in the safety parameters (see AXIS#.SAFEPARAM.SSR_#​.DECMONITOREN).

 

 

This value is t_D_SSR in the following diagram:

Context

For complete SSR information refer to SSR (Safe Speed Range).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Milliseconds

Range

[1, 60000]

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SSR_1.TIMEDELAYDECMONITORING

3161h

07h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_2.TIMEDELAYDECMONITORING

3162h

07h

Unsigned16

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_3.TIMEDELAYDECMONITORING

3163h

07h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_1.TIMEDELAYDECMONITORING

3261h

07h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_2.TIMEDELAYDECMONITORING

3262h

07h

Unsigned16

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_3.TIMEDELAYDECMONITORING

3263h

07h

Unsigned16

-

-

Read/Write

No